Dear Sir/Ms.
Can you check if there is any dynamic load test data? My customer needs 1.8V input 1.5V output load from 0A~0.35A. Spec. need < 0.2V.
Best Regards,
Kami Huang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir/Ms.
Can you check if there is any dynamic load test data? My customer needs 1.8V input 1.5V output load from 0A~0.35A. Spec. need < 0.2V.
Best Regards,
Kami Huang
Hi Kami,
The load transient response depends on multiple application factors including the output capacitor(s), the magnitude of the transient, and the slew rate of the transient. A lower magnitude and slower transient will yield a lower magnitude transient response as the feedback loop will have more time to respond to the transient. A larger output capacitor will reduce the magnitude of the transient as well. Below please find our transient performance as shown in the datasheet. While these do not show your exact conditions, they do demonstrate that the magnitude of the response to a larger transient is less than 100 mV across the range of output voltages.
Very Respectfully,
Ryan