This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM84205: TPSM84205 adjusting the output voltage

Part Number: TPSM84205
Other Parts Discussed in Thread: TPSM84203

Hi all,

I need a DCDC like the TPSM84205 or the TPSM84203, because it follows the TO-220 standard pinout, but I would need to vary the ouput voltage to 3.8-4V. Would it be possible to replace one or both of the feedback resistors to achieve this? When you buy the module, the components are covered with some protection glue or I can have access to them? For most of the DCDC converters the feedback resistors select the output voltage and with such a small variation maybe it does not affect the rest of the module.

Thank you very much for your help in advance