This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441-G1: Minimum measurable current

Part Number: BQ27441-G1

Hi,

Reading the previous questions in the forum I understand that the coulomb counter ADC has an effective resolution of 16 bit and a range of 50mV so each LSB equals 0.76 uV --> with a 10mOhm resistor this equals 76uA (theoretical).

So, Can I read current less than 1 mA (the resolution of AverageCurrent) or can I change the internal ratio of the ADC?

Because I need to read current with resolution near the 50 uA.

Best Regards,

Matteo