Other Parts Discussed in Thread: TPS799, TPS3700
Hi,
I am currently using TPS7A25 for 1.8V output generation from 5V line.
The datasheet mentions that the device has Internal soft-start to limit inrush current. But I could not find the time it takes the output to settle to final value (ramp up time)?
Also does the PG signal goes Low and device is turned Off when the output goes beyond ,say 10% or 15% above the desired Output Voltage. If not, can you suggest any regulator which has this Overvoltage shutdown feature? My Load requirement is 250mA and I need EN and PG features as well.
Regards,
Veerasamy