Other Parts Discussed in Thread: BQ25895, BQ25898D
the BQ25895M has pin for D+ D-,the question is the D+ D- can also connect the MCU with connecting to BQ25895M?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Gary,
There are two solutions for D+/D- connection. one is directly connected together as I mentioned. the other is using external multiplexer as you posted.
I also attached one diagram for your reference. But even BQ25895M open D+/D- pin but there still has few capacitance to impact D+/D- signal quality.
So some customers will use external multiplexer to improve D+/D- signal quality.
And you can use BQ25895M's DESL pin (pin24) to control this multiplexer.
Thanks
Connect the DSEL to a logic rail via 10-KΩ resistor. The pin is normally float and pull-up by external resistor. During Input Source Type Detection , the pin drives low to indicate the device D+/D- detection is in progress and needs to take control of D+, D- signals. When detection is completed, the pin keeps low when MaxCharge™ adapter is detected. The pin returns to float and pulls high by external resistor when other input source type is detected.