Part Number: CSD19538Q3A
Other Parts Discussed in Thread: CSD19538Q2
Hi,
I want to make a constant current LED driver with a MOSFET, shunt, opamp configuratie.
The specs of the LED driver:
- Frequency: ≤100 Hz
- Forward current: 1 A
- pulse duration: ≤ 300 micro seconds
- Source: 48 V
- Forward voltage LED's: 34.5-45 V
- Sense Resistor: 1 ohm
- Pmosfet: max 12.5 W during pulse
- Ambient temperature: 60 degree C
I came up with the schematic underneath Vic is set by a analog output and Pulse sets the frequency and duration of the pulse.
Now my question how can I find a suitable MOSFET that can handle the given power dissipation without the requirement of adding a heat sink.