Other Parts Discussed in Thread: LM5155
Hi
My customer applied the TL1454A and configured it for the following specifications.
Input: 7.4 ~ 8.4v
Output 1: 24V
Output 2: 5V
In the new version of the circuit configuration, you want to configure the output 2 to be BOOST Type at 12V.
On TL1454A Datasheet, output2 is configured as a buck.
Do you have any recommended parts?