Other Parts Discussed in Thread: LM5175, LM2775
Hi ,
I am using LM5175 EVM SV601130B - My input voltage range is 3.7V to 4.3V. I have changed the enable resistor divider resistor R16 to 143K and R13 is 249K - this should allow EVM to start at minimum input of 3V .
The problem I am seeing is that it doesn't turn on till the voltage is at 4.35V - why is that happening?