My customer would like to check if they could remove the R3/C5 which connected to SS pin for soft start control if there is no specific SS time requirement in their design? They would like to use in very space limited design. Please help to check
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My customer would like to check if they could remove the R3/C5 which connected to SS pin for soft start control if there is no specific SS time requirement in their design? They would like to use in very space limited design. Please help to check
Hi Minqui,
The application is Vin=3V~5V to 12.5Vout@0.1A but they are still in schematic stage and no inrush information yet. Could you help to check if we could comment based on the condition?