Hi,
I have a DC DC converter design using TPS54060. Input voltage is 37V nominal, 30-42 range. I have set UVLO limits for STOP @ 30V and for START @ 31.5V.
Resistor values are accordingly: 499k and 20k.
However I am verifying important deviations from these limits (sometimes STOP goes as low as 27V).
Is there anything else I should check to achieve consistent results on these limits?
Vout = 5V
Fsw = 700kHz
Thanks, rgds,
Richard