Hi,
Customer used 250mAh battery. Test with below 3 conditions.
1. Set R_ISET=3.9K ohm and got the Iout=214mA. Charger BQ24014 failed to charge when the connected battery voltage is 0V. Then disconnected the system load, the charger was able to charge the 0V battery with charge current 213mA.
2. Tested with R_ISET change to 1K ohm and got the Iout=837mA. The system load connected, the charger was able to charge the 0V battery with charge current 400+mA. But this charge current has over battery spec.
3. Tested with R_ISET=1.8K ohm which is the max value can charge to the 0V battery with the system load connected. But the charge current has over 1C.
Please advise how to optimize the R_ISET to get the charge current to 0V battery with the system load connected.
Best regards,
Randy Chen