Hi,
One of our customer is using LMZ23610 Switcher module with enable.
They want the output only when VIN is greater than 21V.
w.r.t Section 8.2.2.2, 12.7 kΩ for RENB and 42.2 kΩ for RENT resulting in a rising UVLO of 5.51 V. Note that this divider presents 4.62 V to the EN input when VIN is raised to 20 V. Here, Raising Threshold Ven(rising) from formula gives 5.42V.
Now, with 12.7 kΩ for RENB and 196.6 kΩ for RENT results in a rising UVLO of 21 V (my desired value). Note that this divider presents 1.274 V to the EN input when VIN is raised to 21 V. Here, Raising Threshold Ven(rising) from formula gives 19.23V.
I am finding some mismatch with formula.
Pl. clarify. requirement is to enable the output when V input crosses 21V.