Other Parts Discussed in Thread: TPS2042B, TPS2041B
Hi team,
I received following questions from my customer. Could you answer for the questions below today(your time)? Customer would like to have the answer as soon as possible. Sorry to rush you.
1. I think that the TPS2054B can drive 500mA continuous current per channel.
When the all 4 channels are used at the same time, is the device able to drive total 2A(=500mA x 4 channels)?
2. The d/s describes that the current limit is 1A(typ) per channel.
If the all 4 channels are hit current limit, the total current would be 4A(1A(typ) x 4 channels). Is the device able to handle the 4A?
3. If 800mA continuous current flowed for each channel 1 and 2, the total current will be 1.6A. Is there any problem?
Regards,
Yamaguchi