This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160A: Examination of isolated power supply

Part Number: LM5160A

Hi,

I am considering the following specifications for an isolated power supply.
I would like to use the LM5160A device, but is there a reference design with the following specifications?
Are there any devices other than the LM5160A?

(Specification 1)
VIN: 12V
VOUT: 9V
POUT: 1 W
(Specification 2)
VIN: 12V
VOUT: ± 9 V
POUT: 2W
Best regads,