Part Number: TPS62142
Hi,
I would like to enquire about the threshold levels for the TPS62142RGTT (DC/DC converter) EN input. It is not clearly specified in the "TPS6214x3-V to 17-V 2-A Step-Down Converter in 3 × 3 QFN Package" document.
What I gather from the table in Chapter 7.5 of this document, the input is considered high if the applied voltage Vh is 0.65V (typical) to 0.9V (minimum)?! And is considered low if Vl is 0.45V (typical) to 0.3 (minimum)?!
So how to interpreted this? What the EN input voltage should be to Enable the DC/DC converted and what it should be to Disable the converter?
My problem is that my external 15V power supply, after being switched off, still holds about 5V for a while and causes incorrect shutting down of my device which uses internally TPS62142RGTT and TPS62143RGTT DC/DC converters.
The two DC/DC converters are so good that they could keep my device ON. even when the external power supply is OFF for quite some time. As a consequence I also experience HW reset, when the external power supply is switched off instead of full shut-down.
As a potential solution I would like to connect the EN inputs of the DC/DC converters to a voltage resistor divider, so when the external power drops below certain level (5V for example), the DC/DC converters to be disabled.
Please, advise!
Thank you for your help!
Best regards,
Nick