This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5161-Q1: Output Capacitor Selection and Input Capacitor Selection

Part Number: LM5161-Q1

Hello,

Please i need your support


I have 2 questions.


1. Question:

8.2.1.2.5 Output Capacitor Selection:
they have ripple voltage ΔVO = 10 mV, how do you get there?

for my application which value should I take?

 

2. Question:

8.2.1.2.8          Input Capacitor Selection

they have worst case input ripple of ∆VIN, ripple.= 0.5V, and D = 0.5

how do you get there?

 

for my application which value should I take ∆VIN, ripple and D?

 

my application:

Vin,max=60V

Iout,max=0.5

Vout= 15 V

 

Thanks for your Support