This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC39002: UCC39002 or UC3907 for output shunt for sense pin

Part Number: UCC39002
Other Parts Discussed in Thread: UC3907

 Dear TI friends:

I have a qurestion,so canyou help solve it? for  UCC39002  or UC3907,  I want to connect multiple power supplies with Sense function into shunt output, I wonder if it is ok?

Thank you!

  • Hello Frank,
    Please use the UCC39002 for your application.
    The UC3907 is an older part and not used in new designs. The UCC39002 has advanced features, better characteristics and easier to use.
    The UCC39002 has many reference designs and a calculator tool available.
    Regards
    John