1. The BQ24005 has two status indicators stat1 and stat2. In a fault case the stat1 is pulsed and stat2 is off. What is considered as a fault case?.
2. Does temperature fault on the THERM pin fall under this fault condition? What is considered as a thermal shutdown?
3. Is it the shutdown caused due to the internal die temperature?
4. Do you have a reference design showing how to interface this charger with a microcontroller? Is there any other recommended linear charger that has all the features as the BQ24005?