This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1117: tlv1117 alternatives

Part Number: TLV1117
Other Parts Discussed in Thread: TLV767

Hi Team,

Do we have low cost pin-to-pin LDOs to substitute 1117 LDOs with input voltage stress higher than 10V, except for TLV1117? Thanks!

Yang

  • Yang,

    We do not share detailed pricing information on the external forums other than the 1 Ku pricing which is available on TI.com.

    Regarding your request, can you provide additional details about the system/application needs here? What package is the customer currently using (SOT-223, TO-252, TO-220, etc)? The traditional 1117 linear regulator comes is many different package options. Can you also clarify what the load current requirements are here (max current, average load current, etc)?

    One option to consider here would be the TLV767, which is a recently introduced, next generation 1-A, wide-input voltage linear regulator. The TLV767 delivers many advantages over the traditional, standard linear regulator including:

      • Reduced Standby Power:  

        • 50 µA IQ (<10% of previous generation IQ)

        • No minimum load required to achieve proper regulation/stability

      • Superior electrical performance:

        • 1% output voltage accuracy across line, load, and temp (-40 to 125 C)

        • Excellent ripple rejection: 53db PSRR at 100 kHz. 

      • Simple, easy-to-use solution:

        • Ceramic cap stable with minimal input capacitance. No need for tantalums.

        • Foldback current limiting to help enable safe low power circuits

        • Reduced inrush current to deliver a controlled, stable startup

      • Improved thermals in a compact package (4 mm2):

        • θJA=77.7°C/W in 2x2 WSON package

      

  • Hi Soileau,

    TLV767 is also my choice, I just want to make sure if we have better choice with lower cost. thanks!

    Yang