Dear Sirs!
I have a 14,5VDC power supply, I put the TSP25910 in series with it. I have some small load on the TPS25910's output and there is a big one: 14,5V/2,2A. I set the current limit to 3,5A
Unfortunately this load made the chip to be hot - 125°C
I don't really understand the datasheet and the EVM document: I thought that the IC could have 3-20VDC output at 5A as I see in the EVM's documents schematic on page 3.
In contrast with this in the datasheet I see that there is a Power limit 3-7.5W on page 4. and there is a Power limit vs Junction temperature Figure 3. on page 8. and there is a Maximum load at startup on page 17. (it means to me that 12W could power up...)
So what is the truth? Did I misunderstand the power handle capacity of this chip? Could I use it for my 14.5VDC/2.2A load or not?
Please help me!
Regards: Zsolt