This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61322: TPS613222ADBVR max. output current @ 5V Vout

Part Number: TPS61322
Other Parts Discussed in Thread: TPS61022

Dear Sir/Mam

Kindly guide us for TPS613222A part. we have some query regarding this part.

Input voltage apply through the Li-ion battery Vin range is 3.7V to 4.2V 

1. Can I use the TPS613322 for input voltage from 3.7 to 4.2V and output voltage from 5V @ 1.8A current?

2.  Schottky diode is necessary for 5V@1.8V design? kindly suggest a suitable diode part for design 

3. What is Iq for 5V Vout design?

We are waiting for your response.