This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3880-Q1: maximum pull up resistor for LM3880-Q1

Expert 3210 points
Part Number: LM3880-Q1
Other Parts Discussed in Thread: LM3880

Hello team,

My customer wants to decrease quiescent current at standby situation for LM3880-Q1.

LM3880-Q1 output should be 'L' at standby.

So, The current is needed not only LM3880-Q1 Iq but also though external pull up resistor current.

The datasheet mentions to use 100kohm.

However, the customer wants to decrease the current.

Could you please provide the maximum pull up resistor value for decreasing the current?

Best Regards,