Other Parts Discussed in Thread: LM43602, LM43602-Q1
Hi team.
My customer designed reset circuit as the below.
They added pull-up resistor(R2 : 4.7kohm) between SENSE to /MR.
If MCU does not control /MR(/MR input signal is High) and when output voltage of LM43602 is stable, could additional pull-up resistor cause problems with the output?
Could pull-up resistor have a bad effect on the circuit?
Please refer to LM43602-Q1 circuit below.
Please check and reply ASAP.
Thank you