This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65632: what's the difference between TPS65632 and TPS65632A?

Part Number: TPS65632


Hi TIers,

      As the title mentioned, which version should I suggest customer to use? could you please help to tell us, what's the difference between TPS65632  and TPS65632A? TKS.

  • Hi,

    I have notified our expert regarding this topic. Please expect a response by 4/24/19.

    Thanks,

    Aaron

  • Hello Jerry,
    Sorry about the delay in response as it seems that there were some routing issues with this thread.
    The difference between TPS65632 and TPS65632A is that TPS65632 has two selectable levels for AVDD (OUTP2) output: 5.8V or 7.7V based on the voltage level at the SELP2 pin 5. For TPS65632A, AVDD (OUTP2) voltage level is fixed at 7.7V.
    If customer application is for AVDD=7.7V, I would recommend using TPS65632A.

    Kind Regards,
    Liaqat