Hello!
Please could you help me to get answer on the questions about working of TPS61222?
1. What is the current at the FB input in “disable” (Ven = 0) and “enable” (Ven = Vin) modes at a voltage of 5 V at this input?
2. What is the resistance of the internal divider connected to the input FB?
Thank you!
Is this issue pertaining to a military application? :: no
Is this issue pertaining to an automotive application? :: no