This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61222: Is there a pin compatible version of the TPS61220/TPS61222 without pass-through?

Part Number: TPS61222
Other Parts Discussed in Thread: TPS61220,

The circuit is seeing an inrush current of up to 200mA when enabled, which is causing a significant voltage drop on the Alkaline batteries powering the circuit.  This is causing a brownout reset on the MCU when Vcc dips below 1.8VDC.  This occurs when the 2 series alkaline batteries are at 2.85VDC or below.  I need these batteries to work down to 2.0VDC.

The issue is due to the series resistance of the batteries (and/or path between batteries and inductor) being too high for the inrush. 

Any ideas on how to solve this? 

  1. Is there a pin compatible version of the TPS61220/TPS61222 without pass-through?

how low can the value of the cap tied to Vout be (if this could help)?  Currently 4.7uF.