Other Parts Discussed in Thread: UCC27511A
Hello,
I am working on a gate driver design and have two questions. Can you help please?
1. The section 7.1 absolute max ratings of the UCC27524A datasheet shows that source/sink current should not exceed 5A for 0.5us. Can the device handle higher current for shorter duration as long as the I*I*t is within 5A*5A*0.5us = 12.5 A*A*us? For example, can the device operate safely with 6A for 10ns (0.36 A*A*us)?
2. The MSOP-powerPAD package of UCC27524ADGNR has exposed mental pad on the top case. Datasheet mentioned that the bottom pad is connected to device substrate but doesn't mention the top pad. Is the top pad electrically or thermally connected to the internal device? How effective can it be if a heatsink is mounted on the top pad? Is it electrically safe to connect the top pad to GND?
Thank you.
Best regards,
Zhenyu