The question is about using CSD86311W1723 in a Bidirectional Power Switch as in "Figure 7. BPS Configuration – Back-to-Back Connected N-MOSFETs in Common-Source Configuration" of TI Appnote slva948.pdf for Vin in the range of 1.8V to 3.8V and small current in the range of 100nA to 15mA.
This power switch is used in a test board to switch on and off the power to the test circuit. It seems that this Dual N-Channel Power MOSFET CSD86311W1723 was damaged sometimes. The question is whether this could be caused by 1) possible short-circuit/startup inrush current resulted in thermal protection problem, 2) ESD, or something else.
Any suggestion to the reason of the damage?
.