Other Parts Discussed in Thread: LMR62014
I am using the LM2577 to boost a 12V battery to a 15V supply (0.7Amax). The circuit is pretty much your typical circuit and all works fine 99% of the time. Occasionally upon powering up the IC locks up at about 2.8V. I believe that the problem is due to the main power switch between the battery and circuit bouncing and may be causing the LM2577 to go into under voltage lockout.
Given the information above do you agree that the LM2577 is locking up in undervoltage? Is there anyway to prove it? Have you a tried and tested means to avoid the locking up?
Thanks
Paul