I have the same problem as per the linked question. The LM3488 runs for about 3mS when enabled, then switches the FET (Q1) on at 100%.
The connections and part values are as per the diagram, with the correction on R21 to VIN implemented.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have the same problem as per the linked question. The LM3488 runs for about 3mS when enabled, then switches the FET (Q1) on at 100%.
The connections and part values are as per the diagram, with the correction on R21 to VIN implemented.
Hi Garrett,
The conditions on start up are stable. Initial testing was without any load. Tested with a combination of charged battery supply (7.6V and was well in excess of 5A being drawn with no load.)
The other supply was 12.8V current limited to 2.5A, and the current limit was being reached. (has a decent output capacitor and can deliver the peak current needed to start the supply)
I also tried starting with a 120R resistor as a load (should max out at 100mA), and the result was the same.
The output voltage peaks at approx 2.7V but drops back to about 2.2 volts and is steady. (for the time connected which is limited because things start getting very hot)
The input voltage to the circuit drops to 5.6V on the battery supply (batteries themselves reaching supply limits), and drops to 4.1V on the current limited supply.
I assembled a second prototype board to use as a comparison and have identical results.
I've used the LM3488 on several other projects without any real issues (selected again due to having stock here and I like its flexibility), however this is the first coupled coil one I have done.
As per previous designs it is based on the web bench design but I added the enable option as I need to be able to turn it off and on, on demand for maximum efficiency. (intended duty cycle of load is 10-15Sec once or twice a day at peak load and 2 hours at 1A every 6-12 months.)
Thanks
Hi Garrett,
sorry about the delay, I have just returned from 2 weeks away.
I had tried shorting the FET (Q2) to pull R18 directly to ground. This made no difference to the operation.
It appears the LM3488 tries to fire up initially, and the output switches as expected for the 3mS (approx 500nS on pulses). After the 3mS its stops oscillating, however the output is high rather than the expected low if there is an error.
Regards
Ken
Hi Garrett,
We found the problem. The input impedance of our test power supply and battery source had a temperature dependent joint in the wire. On start-up when the LM3488 was switching the FET the increase in load current was pulling the voltage on Vin lower. After about 3mS it was observe that Vin would spike below 4.4V (maybe for 15-20nS) and the LM3488 would lock up. Once locked up the FET was hard on and shorting the battery or power supply and just holding Vin at 4.4V so it never "unlocked" or reset.
We replaced the offending wire and we then observed a reliable start up.
Now we just need to work out why the coil gets so hot at full load but that another topic.
Thanks for your assistance.