This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28C42: Voltage drop

Part Number: UCC28C42
Other Parts Discussed in Thread: TLV431, TL431

Hello,

I have designed a power supply for following specifications on webench.

Vin: 165V to 265V @ 50Hz

Vout: 12V 

I_out_max: 5A

without load I am getting exact 12V at output. But after connecting the load of 2.5A, My voltage is droping to 9.5V. 

What are the possible resons for this to happen? I have assembles 4 cards getting issue only in 1 board.

Regards

Vishal Kakade