Other Parts Discussed in Thread: TUSB217
Hi,
On a laptop product, the USB type-A connector will be place on a daughter card with 190mm FFC cable connected to the system main board. Where would you suggest to implement TPS2544? On daughter card closed to USB connector or on the system main board? The total USB data length would be around 77600mils and the max current rating from this port on VBUS is around 2.1A.
THanks!
Antony