Hello,
I have some question about design for this BQ76PL455A-Q1 IC.
1. VP pin:this pin is for internal regulator(A/D), can I use this pin to another IC that the supply current is about 10 mA ?
2. In Daisy Chain structure, VIO pin should connected to the VDD pin which is belong to the MCU.
Is this design for the transmission of TX、RX、WAKEUP、FAULTN signal ? If yes, can I use an isolation IC to transport these four signals, and leave the VIO pin and VDD pin be separated?
3. The use of our product is cell monitor in Automotive, so we should design like the Figure.34 in the spec., how to choose the value of common mode filter、isolation capacitor、resistance ?
By the way, I want to know is there any practical applications on Daisy Chain for Automotive battery monitor about this BQ76PL455A-Q1 IC?
Look forward to your reply as soon as possible, thank you.