Hi Expert,
Can you help to review the data? I always got the failure report. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
Can you help to review the data? I always got the failure report. Thanks!
Hi Jerry,
No i do not. Our algortithm lead was able to get a valid result with your file, see his response below:
I analysed this case and tried to run with many different min and mas SOC range settings.
What I founds is that there is nothing wrong with the data, but they are difficult to fit and will have higher error
because:
1) wider temperature range, from 60 to -15C (accuracy will always be lower in wider temp range).
2) high voltage chemistry starting with 4.3V, having different shape close to end of discharge
My best result is attached, still not great but much better then what they had.
I used min and max settings of 3 and 8, and a new chemistry file made
for high voltage Li-ion (chemistry type 8).
It is already supported by the tool, but we need to add it to the manual.
The report is attached.
thanks
Onyx