Hi Support,
Pin 1 - EN – directly connected with Vin 1.8V ~ 2.4V, without 10K pull up resistor.
Pin 8 –PS – disable Power saving mode, Pull up 10K with Vin : 1.8V ~ 2.4V.
Result :
VIN :2V, ILOAD: No Load VOUT : 4.47V
VIN :2V, ILOAD: 500mA VOUT : 3.66V
VIN :2V, ILOAD: 550mA VOUT : 3.29V
VIN :2V, ILOAD: 600mA VOUT : 2.98V
This is not our expected result. We need the load current aroud 800mA above @ 3.80V.
In addition, could you advise the efficiency vs output current for TPS61029? This is not found in the datasheet.
Thanks.