Hi Everybody!
I have a question about "TPS92640: datasheet Fs: Switching Frequency.
SNVS902A.pdf
TPS92640 datasheet wrote:
”nearly constant switching frequency”
But follow the output current, "switching frequency" is moved widely.
My question is followings :
Q1: Please let me know why move "switching frequency" (how the method of this control).
Q2: Please let me know the method of stop moved "switching frequency".
In case of mainly light load, this is my issue.
It is difficult at "counterplan of EMI"
My customer setting is followings:
1)Fs:200kHz(R_on:31k,C_on:470pF )
2)Vin:48V
3)Iout:0.65A
4)Vout:4V
5)LED:1pcs Vf:2.7~3.2V @0.2A~1.8A
Best Regards
Shing