This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM43603PWPEVM: LM43603 Feedback Resitor

Part Number: LM43603PWPEVM

Hi Team。 

The explanation on DATASheet is as follows.

RFBT in the range from 10 kΩ to 100 kΩ is recommended formost applications.

But, The sample circuit in the datasheet is 1 MΩ.

Is there any problem even if the top feedback resistance is 1MΩ?
Best Regard.
  • Hi,

    When increasing the feedback resistance, the current draw on the input decreases. However, the FB node is more susceptible to noise since the current decreases. The layout of the FB resistors should be directly next to the IC, and the trace should be routed away from the switch n ode.

    Please let me know if you have any additional questions.

    Best Regards,
    Katelyn