Other Parts Discussed in Thread: LM66100, TPS2115A
Now we use TPS2105, two-way power switch, one is battery power supply, the other is 3.3V power supply. When the battery power supply is small, the current of 3.3V power supply is 50mA. When 3.3V is electrified, it is always enabled. When 3.3V is electrified, MCU3.3V is supplied by 3.3V. When 3.3V is not available, it is supplied by battery power. Now it is found that in the process of switching, MCU3.3V is pulled down and the single chip reset. The timing of power on this chip can't be controlled. Help me to see if I can solve the reset problem. If it can't be solved, please help recommend the appropriate chip.