Tool/software: WEBENCH® Design Tools
Hi,
i needed a 12V to -12V converter with 0.5A, got this design:
i have 2 things i dont understand in this design and will be happy if you could explain them:
1. The Cbyp capacitor see 24V and the capacitor recommended by the design is 10uF/6.3v capacitor
2. The EN voltage when input is 12V is -8.8V, the enable threshold of this part is 1.18V
Thanks,
Shlomi