Other Parts Discussed in Thread: BQ500511A, BQ51003, , BQ25101
Hi,
We are using the bq50002A together with the bq500511A as the TX unit in a wireless charging system. On the RX side, we use a bq51003 in combination with a bq25101 to charge a small battery of 60mAh. We noticed that the battery can become quite hot, possibly destroying the battery, if we charge at 1C. We limited the charging current to 0.5C, 30mA, to decrease the power received and minimize heating of the battery. When I did some efficiency measurements, I noticed that the overall system efficiency (USB to battery) is very poor, only around 11%. I noticed in the datasheet of the bq50002A a small graph indicating that the efficiency is indeed very poor at low power.
Are there ways to improve the efficiency significantly for low power, or would you suggest another part that can perform more optimally for such low power requirements?
Thanks!
Wout