Other Parts Discussed in Thread: LM5143-Q1, LM5119
Hi
LM5145 is used in my customer.
now, there is a new project, the power is higher than before, so customer want to use 2 LM5145 parallel.
the input is together, and the output is together.
customer want to achieve interleave and current sharing.
in LM5119 and LM5143-Q1, I see the schematic on two-phase mode operation.
but in LM5145 datasheet, I don't find this information.
could you help to check if LM5145 can support my customer's requirement?
thanks.