Hi team,
MY customer wants to test our device for below 2 items on bench,
(1) Output Clamp Voltage up to 45 V
-> Can we use figure 4 - Single-Pulse Avalanche Energy Test Circuit and Waveforms for (1). Any alternative idea?
(2) Transistor Outputs of 250-mA Continuous Current.
-> They did a quick test using DC power supply, providing 45V and current set to 250mA. It was damaged, so I was guessing the DC source - CV to CC transition probably not limit the current fast enough... Any suggestion how to setup the test (2) properly?
Thanks a lot!
Andrew