Hello:
We are currently evaluating the ADS124S06IPBS ADC and seem to really like some of its features such as its power consumption. This ADC will be used to measure strain gauge loads and its high precision seems to be ideal. Our product is powered off of a coin cell battery (CR1225) 3V and contains a BLE transceiver. We could use 2 batteries in series if need be. I know its best to use an LDO for a regulator but because of its efficiency and the voltage drop from the coin cell(down to 2.2 volts), This is a far from ideal option for us. Even using 2 batteries in series will yield the same issue. So I have been playing around with the TPS61291 boost regulator and connected it to drive AVSS and AVDD on the ADS124S06IPBS Eval board and did not seem to see much of an increase in noise. I am concerned that I may be missing something during my testing and would like to get your opinion on this matter(in using this boost converter) prior to designing a prototype board. Also, I was not able to find any info in the TPS61291 datasheet with regards to calculating its switching frequency. Should I assume its the LC(output C) resonant frequency assuming I use the recommended L(3.3uH) and C(22uF)? Please note we sell 10s of thousands of these products annually and I need to make sure I am not missing anything. If there is a better choice for our application, please feel free to make a recommendation. In sum, Do you recommend on using this regulator or would you have any other recommendation? Your time and effort will be greatly appreciated.
Regards,
WH