hi
I have a project for HV ceiling fan, so I want a solution spec is
Vin: 82VAC~220VAC
Vout: 310VDC
Iout:2A~3A
does TI have any reference design can provide
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Lin
At 200VAC input the peak AC voltage is 311V, so in order to have a 310VDC output a flyback with a transformer is recommended.
One of our PFC boost controllers configured as a flyback like UCC28050 (TM 1 phase) in PMP11155 or UCC28063A (TM 2 phase) in PMP10116 will be our first recommendation.
Best Regards,
Eric