Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High Volt AC/DC for ceiling fan

Other Parts Discussed in Thread: PMP11155, UCC28063A, PMP10116, UCC28050

hi

I have a project for HV ceiling fan, so I want a solution spec is 

Vin: 82VAC~220VAC

Vout: 310VDC

Iout:2A~3A

does TI have any reference design can provide


 

  • Lin

    At 200VAC input the peak AC voltage is 311V, so in order to have a 310VDC output a flyback with a transformer is recommended.

    One of our PFC boost controllers configured as a flyback like UCC28050 (TM 1 phase) in PMP11155 or UCC28063A (TM 2 phase) in PMP10116 will be our first recommendation.

    Best Regards,

    Eric