This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27313: Diode failure

Part Number: LM27313

I am investigating field failure. Diode MBR0520 fail. Failure description - diode voltage drop, measured with Fluke multi-meter in Diode mode, is 1.5 V compared to 0.1 V for the good one. Datasheet for LM27313 recommends to select MBR0520 if the switch voltage is less than 15 V. Does it means voltage on pin 1 or pin 5 of LM27313? Does top LM27313 top marking SRPB indicates that it was manufactured by TI?

 I measured  input voltage on pin 5 - it is 4.6 V.

I also measured voltage on pin 1 - it is pulses with the peak voltage approximately 55 V.