Other Parts Discussed in Thread: TPS650864, LP8733
Hi Team,
Customer want to check if have similar TPS650864 automotive PMIC could suggest ?
Voltage input is 12V
Voltage output as below list
- 1. Buck1 : 5V/3A
- 2. Buck2: 0.85V/7A
- 3. Buck3: 1.1V/1A
- 4. Buck4: 3.3V/1A
- 5. Buck5: 1.25V/1A
- 6. Buck6: 1.8V/1A
- 7. VTT LDO: 0.9V300mA
- 8. LDO1: 1.8V/50mA
- 9. LDO2: 1.8V/500mA
- 10. LDO3: 1.2V/100mA
The Xilinx FPGA is used XAZU2EG-1SBVA484Q.