This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC29002: UCC29002

Part Number: UCC29002

Hi there,

I would like to parallel two isolated DC/DC module with 53 V input voltage, 28 V output voltage, 25 A output current capability by using UCC29002.

Besides remote sense pins (+Sense and -Sense), the products have an output voltage adjust pin (Vadj). This pin can be used to adjust the output voltage above or below output voltage initial setting by using an external resistor.

To increase the voltage the resistor should be connected between the Vadj pin and +Sense pin and to decrease the output voltage, the resistor should be connected between the Vadj pin and –Sense pin.

I'm just wondering how I should connect ADJ pin of the UCC29002 (pin 5)? Should I connect it to Vadj pin of the module?

Thank you very much in advance!

BR,

Ghasem