Hi,
Could you tell me about out put capacitance and reverse voltage condition.
Customers is reading the data sheet below.
Customers are considering installing a super cap on Cout to operate somewhat even if the input voltage is off.
There are two questions.
1.
Are there any problems with installing the 15mF super cap?
Please advise about the stable operation of device.
2.
The state of "Vin=0V or open ,Vout=2.1V " continues for several minutes.
Do reverse voltage conditions damage the TPS61200?
Please contact us if you have any concerns.
And Please let me know if there is a recommended additional circuit example for the Cout discharge circuit.
Regards,
Yusuke