This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62084A: VFB min and max value at 0 - 85 deg

Part Number: TLV62084A

Hi team,

My customer wants to know the VFB deviation at temperature above 0 degree up to 85 degree.

How much is the min/max value of VFB at 0 - 85 degree?

Regards,

Saito 

  • Hi Saito,

    Values for specific temperature range cannot be provided because it is not part of design validation. It is better to recommend to customer to use the values (Vfb min/max values are 0.435V & 0.462V, respectively at Tamb = -40deg.C to 85deg.C) indicated in the datasheet in their design because all parts are guaranteed to meet this spec.


    Best regards,
    Excel